This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • LPCXpresso802 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the WWDT driver demo in the terminal window:

— Time out reset test start — Watchdog reset occurred

— Window mode refresh test start — WDOG has been refreshed! WDOG has been refreshed! WDOG has been refreshed! WDOG has been refreshed! WDOG has been refreshed! WDOG has been refreshed! WDOG has been refreshed! WDOG has been refreshed! WDOG has been refreshed! WDOG has been refreshed!