This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware Requirements

  • Mini/micro USB cable

  • LPCXpresso804 board

  • Personal Computer

Board Settings

No special settings are required.

Run the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP port(CN2 on the board).

  2. Choose an IDE, building the project and download the program to the target board. More information about how to compile and program the project can refer to the

    [Getting Started with MCUXpresso SDK](../../../../docs/Getting Started with MCUXpresso SDK.pdf).

  3. Launch the debugger in your IDE to begin running the demo.

Expected Result

When the demo runs successfully, you will find the LED is blinking.