This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • LPCXpresso804 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a micro USB cable between the host PC and the CMSIS DAP port(CN2 on the board).

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

Running the demo

  1. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

The following lines are printed to the serial terminal when the demo program is executed.

IAP example

PartID: XXXXX

The major version is: XXXX

The minor version is: XXXX

Unique ID: XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

End of IAP Example