This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Functional Description

The example will configure the SWM for PLU inputs, outputs, and clock input, then configure the PLU module to make it work.

Note: The RGB LED in this case turns on when the pin level is low and it turns off when the pin level is high.

Each of the three LUT elements are connected to the three PLU input sources to control the RGB LED.

Hardware Requirements

  • Mini/micro USB cable

  • LPCXpresso804 board

  • Personal Computer

Board Settings

PLU input pins connection:

  • CN3_7 (GPIO0_8) to CN8_2 (PLU_IN2).

  • CN3_6 (GPIO0_9) to CN3_10 (PLU_IN3).

  • CN5_1 (GPIO0_10) to CN8_5 (PLU_IN4).

PLU output pins connection:

  • CN3_1 (PLU_OUT0) to CN8_4 (LED_RED).

  • CN3_8 (PLU_OUT1) to CN8_6 (LED_GREEN).

  • CN5_2 (PLU_OUT2) to CN8_3 (LED_BLUE).

Run the Project

  1. Connect a micro USB cable between the PC host and the CMSIS DAP port(CN2 on the board).

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Choose an IDE, building the project and download the program to the target board. More information about how to compile and program the project can refer to the

    [Getting Started with MCUXpresso SDK](../../../../docs/Getting Started with MCUXpresso SDK.pdf).

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Expected Result

Input source and LED status table:

PLU_IN4

PLU_IN3

PLU_IN2

LED_BLUE

LED_GREEN

LED_RED

0

0

0

off

off

off

0

0

1

off

off

on

0

1

0

off

on

off

0

1

1

on

off

off

1

0

0

off

on

on

1

0

1

on

off

on

1

1

0

on

on

off

1

1

1

on

on

on

The log below shows the output of the plu combination example in the terminal window:

PLU combination driver example.

Select the input source.
1. Input source 0
2. Input source 1
3. Input source 2
4. Set all three input sources.
0
Select the input value.
0. Low level.
1. High level.
1
Select the input source.
0. Input source 0
1. Input source 1
2. Input source 2
3. Set all three input sources.
3
Input the three values like 000.
0. Low level.
1. High level.
011

The LED will change as the description in the table