This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • USB Type-C cable

  • MCIMX93AUTO-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

The example requires doing connection between FLEXIO1(as master) pins and LPI2C1(as slave) pins.

  • LPI2C1_SCL(J17-16), IOMUXC_PAD_GPIO_IO02__FLEXIO1_FLEXIO02(J16-3) connected

  • LPI2C1_SDA(J17-18), IOMUXC_PAD_GPIO_IO03__FLEXIO1_FLEXIO03(J16-5) connected

Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

Prepare the Demo

  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW2 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J26 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

FlexIO I2C example read accelerometer value
Found a LSDM6DSO on board, the device address is 0x6A.
The accel values:
status_reg = 0x5 , x = -28924 , y =  5127 , z = 24640
status_reg = 0x5 , x = 31748 , y =  9991 , z = 27456
status_reg = 0x5 , x = 28164 , y = 14599 , z = 15680
status_reg = 0x5 , x = 24068 , y = 21767 , z = 31808
status_reg = 0x5 , x = 13828 , y = -32505 , z = 22848
status_reg = 0x5 , x = 10500 , y = -26105 , z = 16192
status_reg = 0x5 , x =  6916 , y = -26105 , z = 17472
status_reg = 0x5 , x =  8452 , y = -25081 , z = 21056
status_reg = 0x5 , x =  8964 , y = -26105 , z = 22080
status_reg = 0x5 , x =  7940 , y = -24569 , z = 20800

End of I2C example .