This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • MCX-N5XX-EVK board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:


ERM error recording example.

Original ram data correct.

ERM error recording address is 0x20006000.

ERM error recording example finished successfully.

Note: All system bus masters can access the programming model:

  1. Only in supervisor mode

  2. Using only 32-bit (word) accesses Any of the following attempted references to the programming model generates an error termination:

  3. In user mode

  4. Using non-32-bit access sizes

  5. To undefined (reserved) addresses