This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • MCX-N5XX-EVK board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

ITRC Peripheral Driver Example

Pass: No Event/Action triggered in STATUS after Init

Enable ITRC IRQ Action response to SW Event 0

Trigger SW Event 0

ITRC IRQ Reached! ITRC STATUS: SW Event0 occured! Generated ITRC interrupt!

Clear ITRC IRQ and SW Event 0 STATUS

Disable ITRC IRQ Action response to SW Event 0

Trigger SW Event 0

Pass: No Action triggered

End of example