This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • MCX-N9XX-EVK board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a micro USB cable between the host PC and the MCU-Link USB port (J5) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the CTimer driver simple match demo in the terminal window:

CTimer match example to toggle the output on a match

You can see the green led blinking on board.