Hardware requirements
Mini/micro USB cable
MCX-N9XX-EVK Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Press anykey to start the example...
EWM example
Press SW3 to expire EWM
EWM interrupt is occurred
Press SW3 to expire EWM again