Hardware requirements
Micro USB cable
MCX-N9XX-EVK board
Personal Computer
3.5” TFT LCD module by NXP (P/N PAR-LCD-S035)
Board settings
Attach the LCD shield to the EVK board.
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Build the project.
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
If this example runs correctly, the sample GUI is displayed.