This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • MIMXRT685-AUD-EVK board

  • Personal Computer

Board settings

  • Set VREF_L to GND, VREF_H to 1.8V (connect JP9, JP10).

  • Input voltage signal(0~1.8V) to J30-1(LPADC0 CH0).

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, following information can be seen on the terminal:

LPADC Interrupt Example
Please press any key to get user channel's ADC value.
ADC value: 4093
ADC interrupt count: 1
ADC value: 4095
ADC interrupt count: 2
ADC value: 4093
ADC interrupt count: 3