Hardware requirements
Micro USB cable
MIMXRT685-AUD-EVK board
Personal Computer
Board settings
No special settings are required.
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the SCTimer driver PWM demo in the terminal window:
SCTimer example to output center-aligned PWM signal
You will see a change in LED brightness if an LED is connected to the SCTimer output pin
If no LED is connected to the pin, then probe the signal using an oscilloscope
Observe the green led to see the SCTimer pwm signal.