This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • MIMXRT700-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the freqme_interrupt demo in the terminal window:

FREQME Interrupt Example!
Please select operate mode...
        A -- Frequency Measurement Mode.
        B -- Pulse Width Measurement Mode.
Frequency Measurement Mode Selected!
Please select the target clock:
                A -- OSC_CLK
                B -- FRO1_DIV8
                C -- LPOSC
Please input the scale factor of reference clock(Ranges from 0 to 31).
20
Target clock frequency is 11999725 Hz.
Please select operate mode...
        A -- Frequency Measurement Mode.
        B -- Pulse Width Measurement Mode.