This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • MIMXRT700-EVK board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the USB port on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the GLIKEY driver demo in the terminal window:

GLIKEY Peripheral Driver Example

*Success* GLIKEY is not locked

*Success* GLIKEY Sync Reset done

*Success* GLIKEY Start enable done

*Success* GLIKEY Continue enable Step 1 pass

*Success* GLIKEY Continue enable Step 2 pass

*Success* GLIKEY Continue enable Step 3 pass

*Success* GLIKEY Continue enable Step Enable pass

SUCCESS: Register on index 2 can be now written!

*Success* GLIKEY End of operation done

End of example