This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • MIMXRT700-EVK board

  • Personal Computer

  • RK055AHD091 panel or RK055MHD091 panel

Board settings

Connect the MIPI panel to MIMXRT700-EVK board J105. For single_stream_repeat and context_switch examples, make sure JP65 1-2 are connected, and insert the SD card which has the pictures unziped in root folder in slot J47.

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J54) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Build the project, this project uses RK055MHD091 panel by default, to use the RK055AHD091 panel, change #define DEMO_PANEL DEMO_PANEL_RK055MHD091 to #define DEMO_PANEL DEMO_PANEL_RK055AHD091 in display_support.h.

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs, the screen shows what described in overview.