This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • TFT Proto 5” CAPACITIVE board HW REV 1.01 by Mikroelektronika. (Named as SSD1963 panel in project. Not necessary if use MIPI panel)

  • MIMXRT700-EVK

  • Personal Computer

  • RK055AHD091 MIPI panel (Not necessary if use other panel)

  • RK055MHD091 MIPI panel (Not necessary if use other panel)

  • RaspberryPi Panel (Not necessary if use other panel)

Board settings

To use SSD1963 panel: Connect SSD1963 panel to J4.

To use MIPI panel: Connect MIPI panel to J52.

To use Raspberry panel: Connect the panel to J8. Then connect the panel’s 5V pin to JP43-1, GND pin to JP43-2.

Prepare the Demo

The demo use SSD1963 panel by default, to use MIPI RK055AHD091 panel, change the macro DEMO_PANEL to DEMO_PANEL_RK055AHD091 in display_support.h. To use MIPI RK055MHD091 panel, change the macro DEMO_PANEL to DEMO_PANEL_RK055MHD091 in display_support.h. To use RaspberryPi, change the macro DEMO_PANEL to DEMO_PANEL_RASPI_7INCH in display_support.h.

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J54) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs, the screen shows what described in overview.