Hardware requirements
Micro USB cable
MIMXRT700-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the USB port on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
Gpio toggle demo - message from primary core side. Gpio toggle demo - message from ezhv core side. Press any key to start the program. Ezhv irq channel = 0x1 Ezhv irq channel = 0x1 Ezhv irq channel = 0x1
Connect J6-5 to an oscilloscope to observe a square wave.