Hardware requirements
Micro USB cable
MIMXRT700-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-LINK USB port on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
FATFS example to demonstrate how to use FATFS with MMC card.
Make file system......The time may be long if the card capacity is big.
Create directory......
Create a file in that directory......
List the file in that directory......
General file : F_1.DAT.
Write/read file until encounters error......
Write to above created file.
Read from above created file.
Compare the read/write content.
The read/write content is consistent.
Input 'q' to quit read/write.
Input other char to read/write file again.