This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • RD-RW61X-BGA board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the CRC driver demo in the terminal window:

CRC Peripheral Driver Example

Test string: 123456789
CRC-16 CCITT FALSE: 0x29b1
CRC-16 ARC: 0xbb3d
CRC-32: 0xcbf43926