This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • RD-RW61X-BGA board

  • Personal Computer

  • LCD-PAR-S035 panel

Board settings

  • Short JP3, JP44, JP50

  • Wire R624, R625, R626, R627, R629, R630, R631, R616, R662, R663, R664, R665

  • Connect LCD-PAR-S035 to header J23, J23-1 match LCD J1-1

  • Set the switch SW1 on LCD-PAR-S035 to 011 (IM[2:0), note the left one is IM[0], right one is IM[2].

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the example.

Running the demo

If this example runs correctly, the panel shows as the overview description.