This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • TWR-KM35Z75M board

  • Personal Computer

Board settings

Probe signal at J25-20 using oscillator.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

*********QUADTIMER EXAMPLE START*********
****Timer use-case, 1 second tick.****
 Timer interrupt has occurred !
 Timer interrupt has occurred !
....................
....................
****Chain Timer use-case, 10 second tick.****
 Timer interrupt has occurred !
 Timer interrupt has occurred !
.........
.........
****Input capture example.****
****Provide a signal input to the TMR0 pin****
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Input rising signal at J21-1. Then the following message is displayed:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Input Captured value=bebe

*********Make sure to connect a scope.*********

****A 50 duty cycle PWM wave is observed in the scope.****

*********QUADTIMER EXAMPLE END.*********
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
And you will find the LED RED is taking turns to shine.