This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

cmsis_spi_dma_b2b_transfer_master

Overview

The cmsis_spi_dma_b2b_transfer example shows how to use SPI CMSIS driver in dma way:

In this example , we need two boards, one board used as SPI master and another board used as SPI slave. The file ‘cmsis_spi_dma_b2b_transfer_master.c’ includes the SPI master code.

  1. SPI master send/received data to/from SPI slave in edma way.