This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

cmsis_spi_int_b2b_transfer_slave

Overview

The cmsis_spi_int_b2b_transfer example shows how to use SPI CMSIS driver in interrupt way:

In this example , we need two boards, one board used as SPI master and another board used as SPI slave. The file ‘cmsis_spi_int_b2b_transfer_slave.c’ includes the SPI slave code.

  1. SPI master send/received data to/from SPI slave in interrupt .