This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

hardfault_handling

Overview

The Hardfault Handling demo is used to demonstrate the functionality of the exception handling component. This main function is used to generate a hardfault event. The program enters hardfault when you input the character “1”. Then you can see the “Stack frame” information in the terminal.

Supported Boards