This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lib_jpeg_hw_accel

Overview

The lib jpeg with hardware acceleration demo decodes the JPEG picture using the JPEG decoder hardware, and shows them in the LCD panel. Since not all JPEG formats are supported by the hardware, when macro LIB_JPEG_USE_HW_ACCEL is on, the lib jpeg will parse the header first, if the format is supported, it will use the hardware to accelerate, otherwise will use the old software way.

Supported Boards