This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

ecat_eoe

Overview

This example demonstrates how to use EtherCAT EoE based on digital_io example.

Note that the demo CAN NOT be built directly. Please see the “Prepare the Demo” section for more details. For more information on digital_io example, please refer to ‘.\boards\evkmimxrt1180\ecat_examples\digital_io’

Running the demo

When the example is running, the serial port will output:

Start the SSC EoE example… Hardware init success… EoE interface init success…


HTTP Server example


IPv4 Address : 192.168.1.66 IPv4 Subnet mask : 255.255.255.0 IPv4 Gateway : 192.168.1.102 mDNS hostname : lwip-eoe


NOTE: To modify the html of http server, please refer to lwip_examples/lwip_httpsrv example.

Supported Boards