This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

central_ipsp

Overview

Application demonstrating very basic BLE Central role functionality by scanning for other BLE devices and establishing a connection to the first one with a strong enough signal. Except that this application specifically looks for IPSP Service and communicates between the devices that support IPSP is done using IPv6 packets over the Bluetooth Low Energy transport once connected.

Prepare the Demo

  1. Open example’s project and build it.

  2. Connect a USB cable between the PC host and the OpenSDA USB port on the target board.

  3. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

The demo does not require user interaction. The application will automatically start scanning and will connect to the first advertiser who is advertising the IPSP Service. After the L2CAP credit-based channel specified by the IPSP Profile is established, the application will send a predefined test message every 5 seconds through the channel. Example output:

Sending message...

Supported Boards