tflm_modelrunner
Overview
TFlite Model Behchmark example for Microcontrollers.
Toolchains supported - MCUXpresso IDE - IAR Embedded Workbench for ARM - Keil uVision MDK - ArmGCC - GNU Tools ARM Embedded
Supported board and settings - mcxn9xxevk: HTTP mode(default) UART mode: remove MODELRUNNER_HTTP from cc/cx flags. - mcxn9xxbrk: UART mode.
Running the demo
Get benchmark results via ModelRunner http handler
HTTP Mode:
           TFLite Modelrunner
Initializing PHY… DHCP state : SELECTING DHCP state : REQUESTING DHCP state : BOUND
IPv4 Address : 10.193.20.56 IPv4 Subnet mask : 255.255.255.0 IPv4 Gateway : 10.193.20.254
Initialized TFLiteMicro modelrunner server at port 10818
Upload test model: $ curl -X PUT http://10.193.20.56:10818/v1 -F ‘file=@”/home/x/eiq/model/mlperf_tiny_models/keyword_spotting/kws_ref_model.tflite”;filename=”kws_model;name=block_content”’ && echo {“reply”: “success”}
Run latency benchmark: xiao@x:~/work/eiq$ curl -X POST http://10.193.20.56:10818/v1?run=1 && echo {“timing”:57202000}
Get Model info: xiao@x:~/work/eiq$ curl http://10.193.20.56:10818/v1/model && echo {“timing”:57207000,”inputs”:[{“name”:”input_1”,”scale”:0.58470290899276733,”zero_points”:83,”datatype”:”INT8”,”shape”:[1,49,10,1]}],”outputs”:[{“name”:”Identity”,”scale”:0.00390625,”zero_points”:-128,”datatype”:”INT8”,”shape”:[1,12]}],”layer_count”:13,”layers”:[{“name”:”functional_1/activation/Relu;functional_1/batch_normalization/FusedBatchNormV3;functional_1/conv2d/BiasAdd/ReadVariableOp/resource;functional_1/conv2d/BiasAdd;functional_1/conv2d_4/Conv2D;functional_1/conv2d/Conv2D1”,”type”:”CONV_2D”,”avg_timing”:9275000,”tensor”:{“timing”:9275000}},{“name”:”functional_1/activation_1/Relu;functional_1/batch_normalization_1/FusedBatchNormV3;functional_1/depthwise_conv2d/depthwise;functional_1/depthwise_conv2d/BiasAdd;functional_1/conv2d_4/Conv2D;functional_1/depthwise_conv2d/BiasAdd/ReadVariableOp/resource1”,”type”:”DEPTHWISE_CONV_2D”,”avg_timing”:4379000,”tensor”:{“timing”:4379000}},{“name”:”functional_1/activation_2/Relu;functional_1/batch_normalization_2/FusedBatchNormV3;functional_1/conv2d_1/BiasAdd/ReadVariableOp/resource;functional_1/conv2d_1/BiasAdd;functional_1/conv2d_4/Conv2D;functional_1/conv2d_1/Conv2D1”,”type”:”CONV_2D”,”avg_timing”:7492000,”tensor”:{“timing”:7492000}},{“name”:”functional_1/activation_3/Relu;functional_1/batch_normalization_3/FusedBatchNormV3;functional_1/depthwise_conv2d_1/depthwise;functional_1/depthwise_conv2d_1/BiasAdd;functional_1/conv2d_4/Conv2D;functional_1/depthwise_conv2d_1/BiasAdd/ReadVariableOp/resource1”,”type”:”DEPTHWISE_CONV_2D”,”avg_timing”:4374000,”tensor”:{“timing”:4374000}},{“name”:”functional_1/activation_4/Relu;functional_1/batch_normalization_4/FusedBatchNormV3;functional_1/conv2d_2/BiasAdd/ReadVariableOp/resource;functional_1/conv2d_2/BiasAdd;functional_1/conv2d_4/Conv2D;functional_1/conv2d_2/Conv2D1”,”type”:”CONV_2D”,”avg_timing”:7494000,”tensor”:{“timing”:7494000}},{“name”:”functional_1/activation_5/Relu;functional_1/batch_normalization_5/FusedBatchNormV3;functional_1/depthwise_conv2d_2/depthwise;functional_1/depthwise_conv2d_2/BiasAdd;functional_1/conv2d_4/Conv2D;functional_1/depthwise_conv2d_2/BiasAdd/ReadVariableOp/resource1”,”type”:”DEPTHWISE_CONV_2D”,”avg_timing”:4374000,”tensor”:{“timing”:4374000}},{“name”:”functional_1/activation_6/Relu;functional_1/batch_normalization_6/FusedBatchNormV3;functional_1/conv2d_3/BiasAdd/ReadVariableOp/resource;functional_1/conv2d_3/BiasAdd;functional_1/conv2d_4/Conv2D;functional_1/conv2d_3/Conv2D1”,”type”:”CONV_2D”,”avg_timing”:7490000,”tensor”:{“timing”:7490000}},{“name”:”functional_1/activation_7/Relu;functional_1/batch_normalization_7/FusedBatchNormV3;functional_1/depthwise_conv2d_3/depthwise;functional_1/depthwise_conv2d_3/BiasAdd;functional_1/conv2d_4/Conv2D;functional_1/depthwise_conv2d_3/BiasAdd/ReadVariableOp/resource1”,”type”:”DEPTHWISE_CONV_2D”,”avg_timing”:4380000,”tensor”:{“timing”:4380000}},{“name”:”functional_1/activation_8/Relu;functional_1/batch_normalization_8/FusedBatchNormV3;functional_1/conv2d_4/BiasAdd/ReadVariableOp/resource;functional_1/conv2d_4/BiasAdd;functional_1/conv2d_4/Conv2D1”,”type”:”CONV_2D”,”avg_timing”:7491000,”tensor”:{“timing”:7491000}},{“name”:”functional_1/average_pooling2d/AvgPool”,”type”:”AVERAGE_POOL_2D”,”avg_timing”:397000,”tensor”:{“timing”:397000}},{“name”:”functional_1/flatten/Reshape”,”type”:”RESHAPE”,”avg_timing”:5000,”tensor”:{“timing”:5000}},{“name”:”functional_1/dense/BiasAdd”,”type”:”FULLY_CONNECTED”,”avg_timing”:24000,”tensor”:{“timing”:24000}},{“name”:”Identity”,”type”:”SOFTMAX”,”avg_timing”:27000,”tensor”:{“timing”:27000}}]}
Upload input tensor and get output tensor data: $ curl -s -X POST “http://10.193.20.56:10818/v1?run=1&output=Identity” -F’file=@”/home/x/eiq/benchmark-runner-ml/datasets/kws01/tst_000337_Yes_9.bin”;filename=”input_tensor;name=input_1”’ |jq .outputs[0].data | xargs -i echo {$i} |base64 -d | hexdump -C 00000000 80 80 80 80 80 80 80 80 80 7f 80 80 |…………|
$ curl -s -X POST “http://10.193.20.56:10818/v1?run=1&output=Identity” -F’file=@”/home/x/eiq/benchmark-runner-ml/datasets/kws01/tst_000301_Left_2.bin”;filename=”input_tensor;name=input_1”’ |jq .outputs[0].data | xargs -i echo {$i} |base64 -d | hexdump -C 00000000 80 80 7f 80 80 80 80 80 80 80 80 80 |…………|
UART Mode:
Download the program to the target board.
Use the scripts scripts/main.py to launch the http service on x86 platform to handle the http requests and forward the data to the board via uart. #python3 main.py
Serving Flask app “main” (lazy loading)
Environment: production WARNING: This is a development server. Do not use it in a production deployment. Use a production WSGI server instead.
Debug mode: on
Running on http://0.0.0.0:10919/ (Press CTRL+C to quit)
Restarting with stat
Debugger is active!
Debugger PIN: 132-343-000
Connect the uart cable to x86.
The uri should be http://localhost:10919/serial/
Do benchmark testing with deepview-validator or eIQ Model Tool:
DeepviewRT validator: #deepview-validator –input_names input –output_names MobilenetV1/Predictions/Reshape_1 –samples 1 –uri http://localhost:10919/serial/GRAXBQHR
–reference mobilenet_v1_1.0_224_pb.npz mobilenet_v1_1.0_224_pb_uint8.tfliteeIQ Model Tool: Add target with uri ‘http://localhost:10919/serial/GRAXBQHR’ and click the ‘Tools->Profile Model’ button to to profiling model.
Get benchmark results via Modelrunner cli
PS C:\scripts> python .\cli.py com20
=> reset
           TFLite Modelrunner
=> model_loadb model.tflite model_loadb 53936 ######### Ready for TFLite model download Flash FLASH 0x100000 Erased, Program at 100000: 16384 bytes == FLASH 0x104000 Erased, Program at 104000: 16384 bytes == FLASH 0x108000 Erased, Program at 108000: 16384 bytes == FLASH 0x10c000 Erased, Program at 10c000: 16384 bytes ==
=> model
{
“inputs”: [
{
“datatype”: “INT8”,
“name”: “input_1”,
“scale”: 0.5847029089927673,
“shape”: [
1,
49,
10,
1
],
“zero_points”: 83
}
],
“layer_count”: 13,
“layers”: [
{
“avg_timing”: 9827000,
“name”: “functional_1/activation/Relu;functional_1/batch_normalization/FusedBatchNormV3;functional_1/conv2d/BiasAdd/ReadVariableOp/resource;functional_1/conv2d/BiasAdd;functional_1/conv2d_4/Conv2D;functional_1/conv2d/Conv2D1”,
“tensor”: {
“timing”: 9827000
},
“type”: “CONV_2D”
},
…
…
],
“outputs”: [
{
“datatype”: “INT8”,
“name”: “Identity”,
“scale”: 0.00390625,
“shape”: [
1,
12
],
“zero_points”: -128
}
],
“timing”: 60370000
}
=> tensor_loadb input_1 tmp.input tensor_loadb input_1 490 ######### Ready for input_1 tensor download MEM
######### 490 bytes received #########
=> run output=Identity { “outputs”: [ { “data”: “gICAgICAgIB/gICA”, “datatype”: “INT8”, “name”: “Identity”, “shape”: [ 1, 12 ], “type”: “SOFTMAX” } ], “timing”: 59808000 }
=>
The latency timing is 59.808 ms, the layer timings can be found in model command, for example the first layer timing is 9.827 ms.