This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

EdgeLock 2GO MQTT Demo (S)

This demo demonstrates how to use MQTT connections to cloud services such as AWS or Azure with preprovisioned keys and certificates from the EdgeLock 2GO service.

The workspace structure (when building this order must be respected):

  • el2go_mqtt_demo_s: project running in Secure processing environment (SPE)

  • el2go_mqtt_demo_ns: project running in Non-secure processing environment (NSPE)

Details on building and running the application are included in the el2go_mqtt_demo_ns readme

Hardware requirements

  • FRDM-RW612 or RD-RW61X-BGA board

  • USB-C (FRDM-RW612) or Micro-USB (RD-RW61X-BGA) cable

  • Personal Computer

Board settings

No special settings are required.