This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

ele_crypto_generic_rsa

Overview

The ELE Crypto Generic Example project is a demonstration program that uses the MCUX SDK software to perform generic crypto operations usign plaintext key with EdgeLock Enclave (ELE).

Running the demo

Example output on terminal:

EdgeLock Enclave secure Sub-System Driver Example:

*********** Load EdgeLock FW ****************************** EdgeLock FW loaded and authenticated successfully.

****************** Start RNG ****************** EdgeLock RNG Start success. EdgeLock RNG ready to use.

*********** Generic Crypto RSA keygen ********************* RSA Key-Pair generation. RSA Key-pair generated successfully.

*********** Generic Crypto RSA PKCS#1.5 Signature gen ***** RSA signature with input as digest generated successfully. RSA signature with input as message generated successfully.

*********** Generic Crypto RSA PSS Signature gen ********** RSA signature generated successfully.

*********** Generic Crypto RSA 2048 PKCS#1.5 Verify ******* RSA verify success

*********** Generic Crypto RSA 3072 PSS Verify ************ RSA verify success

*********** Generic Crypto RSA PKCS#1.5 encrypt *********** RSA encryption success.

*********** Generic Crypto RSA PKCS#1.5 decrypt *********** RSA decryption success, plaintext match original one.

*********** Generic Crypto RSA OAEP encrypt *************** RSA encryption success.

*********** Generic Crypto RSA OAEP decrypt *************** RSA decryption success, plaintext match original one.

End of Example with SUCCESS!!

Supported Boards