This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

freertos_blinky_s

Overview

This document explains the freertos_tzm example. This demo application utilizes TrustZone, so it demonstrates following techniques for TrustZone applications development:

  1. Application separation between secure and non-secure part

  2. TrustZone environment configuration

  3. Exporting secure function to non-secure world

  4. Calling non-secure function from secure world

  5. Configuring IAR, MDK, GCC and MCUX environments for TrustZone based projects

Running the demo

The Trust Zone-M (TZM) demo creates two unprivileged tasks. One of which calls a secure side function and passes a pointer to a callback function. The secure side function does three things:

  1. It calls the provided callback function. The callback function increments a counter.

  2. It increments a counter and returns the incremented value. After the secure function call finishes, it verifies that both the counters are incremented.

  3. It calls a secure side function to toggle the green LED The second task just calls a secure side function to toggle the blue LED

Supported Boards