This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lwip_dhcp_enet_qos_freertos

Overview

The lwip_dhcp demo application demonstrates a DHCP demo on the lwIP TCP/IP stack.The application acts as a DHCP client and prints the status as it is progressing.Once the interface is being bound to an IP address obtained from DHCP server, address information is printed.

Supported Boards