This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lwip_iperf_enet_qos_bm

Overview

This is the IPerf server example to check your bandwidth using the network performance measurement IPerf application on a PC as a client.It is currently a minimal implementation providing an IPv4 TCP server only.Instead of the command line IPerf application, for more convenience, it is recommended to use the JPerf2 graphical tool, which can be downloaded here: https:/sourceforge.net/projects/iperf/files/jperf/jperf%202.0.0/jperf-2.0.0.zip/download

Supported Boards