This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lwip_mqtt_enet_qos_freertos

Overview

The lwip_mqtt demo application demonstrates MQTT client connecting to MQTT broker via unsecured socket. The application obtains IP and DNS addresses from DHCP and resolves broker’s hostname if needed. Then it connects to the broker and subscribes to the “lwip_topic/#” and “lwip_other/#” topics. Further it publishes five messages to the “lwip_topic/100” which are also received back as the board is subscribed to the “lwip_topic/#”. Meanwhile it continues to receive messages published to the subscribed topics from other clients.

Supported Boards