This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

mbed-crypto_benchmark

Overview

The Mbed-Crypto demo application performs cryptographic algorithm benchmarking and prints results to the terminal.

Prepare the Demo

Connect a serial cable from the debug UART port of the target board to the PC. Start TeraTerm (http://ttssh2.osdn.jp) and make a connection to the virtual serial port.

  1. Start TeraTerm.

  2. New connection -> Serial.

  3. Set the appropriate COMx port (where x is port number) in the port context menu. The number is provided by the operating system, and could be different from computer to computer. Select the COM number related to the virtual serial port. Confirm the selected port by clicking the “OK” button.

  4. Set following connection parameters in menu Setup -> Serial port. Baud rate: 115200 Data: 8 Parity: none Stop: 1 Flow control: none

  5. Confirm selected parameters by clicking the “OK” button.

Running the demo

When the demo runs successfully, which takes a couple of minutes, the terminal displays similar information like the following:

MD5 : 3528 KiB/s, 26 cycles/byte RIPEMD160 : 1295 KiB/s, 72 cycles/byte SHA-1 : 1712 KiB/s, 54 cycles/byte SHA-256 : 855 KiB/s, 109 cycles/byte SHA-512 : 491 KiB/s, 190 cycles/byte ARC4 : 5163 KiB/s, 18 cycles/byte 3DES : 83 KiB/s, 1149 cycles/byte DES : 241 KiB/s, 389 cycles/byte 3DES-CMAC : 79 KiB/s, 1198 cycles/byte AES-CBC-128 : 2 KiB/s, 134 cycles/byte AES-CBC-192 : 605 KiB/s, 154 cycles/byte AES-CBC-256 : 539 KiB/s, 173 cycles/byte AES-XTS-128 : 610 KiB/s, 153 cycles/byte AES-XTS-256 : 486 KiB/s, 192 cycles/byte AES-GCM-128 : 344 KiB/s, 271 cycles/byte AES-GCM-192 : 321 KiB/s, 291 cycles/byte AES-GCM-256 : 301 KiB/s, 311 cycles/byte AES-CCM-128 : 310 KiB/s, 302 cycles/byte AES-CCM-192 : 274 KiB/s, 342 cycles/byte AES-CCM-256 : 246 KiB/s, 380 cycles/byte ChaCha20-Poly1305 : 513 KiB/s, 182 cycles/byte AES-CMAC-128 : 622 KiB/s, 150 cycles/byte AES-CMAC-192 : 2 KiB/s, 170 cycles/byte AES-CMAC-256 : 493 KiB/s, 189 cycles/byte AES-CMAC-PRF-128 : 619 KiB/s, 150 cycles/byte CAMELLIA-CBC-128 : 323 KiB/s, 290 cycles/byte CAMELLIA-CBC-192 : 248 KiB/s, 377 cycles/byte CAMELLIA-CBC-256 : 249 KiB/s, 377 cycles/byte ChaCha20 : 659 KiB/s, 141 cycles/byte Poly1305 : 2925 KiB/s, 31 cycles/byte BLOWFISH-CBC-128 : 823 KiB/s, 113 cycles/byte BLOWFISH-CBC-192 : 823 KiB/s, 113 cycles/byte BLOWFISH-CBC-256 : 823 KiB/s, 113 cycles/byte CTR_DRBG (NOPR) : 533 KiB/s, 175 cycles/byte CTR_DRBG (PR) : 378 KiB/s, 248 cycles/byte HMAC_DRBG SHA-1 (NOPR) : 120 KiB/s, 785 cycles/byte HMAC_DRBG SHA-1 (PR) : 111 KiB/s, 849 cycles/byte HMAC_DRBG SHA-256 (NOPR) : 89 KiB/s, 1067 cycles/byte HMAC_DRBG SHA-256 (PR) : 89 KiB/s, 1067 cycles/byte RSA-1024 : 0 public/s RSA-1024 : 0 private/s DHE-2048 : 0 handshake/s DH-2048 : 0 handshake/s DHE-3072 : 0 handshake/s DH-3072 : 0 handshake/s ECDSA-secp521r1 : 2 sign/s ECDSA-brainpoolP512r1 : 0 sign/s ECDSA-secp384r1 : 4 sign/s ECDSA-brainpoolP384r1 : 0 sign/s ECDSA-secp256r1 : 5 sign/s ECDSA-secp256k1 : 5 sign/s ECDSA-brainpoolP256r1 : 0 sign/s ECDSA-secp224r1 : 8 sign/s ECDSA-secp224k1 : 0 sign/s ECDSA-secp192r1 : 0 sign/s ECDSA-secp192k1 : 0 sign/s ECDSA-secp521r1 : 1 verify/s ECDSA-brainpoolP512r1 : 0 verify/s ECDSA-secp384r1 : 1 verify/s ECDSA-brainpoolP384r1 : 0 verify/s ECDSA-secp256r1 : 2 verify/s ECDSA-secp256k1 : 2 verify/s ECDSA-brainpoolP256r1 : 0 verify/s ECDSA-secp224r1 : 3 verify/s ECDSA-secp224k1 : 2 verify/s ECDSA-secp192r1 : 3 verify/s ECDSA-secp192k1 : 0 verify/s ECDHE-secp521r1 : 0 handshake/s ECDHE-brainpoolP512r1 : 0 handshake/s ECDHE-secp384r1 : 1 handshake/s ECDHE-brainpoolP384r1 : 0 handshake/s ECDHE-secp256r1 : 2 handshake/s ECDHE-secp256k1 : 2 handshake/s ECDHE-brainpoolP256r1 : 0 handshake/s ECDHE-secp224r1 : 3 handshake/s ECDHE-secp224k1 : 2 handshake/s ECDHE-secp192r1 : 4 handshake/s ECDHE-secp192k1 : 3 handshake/s ECDHE-Curve25519 : 1 handshake/s ECDHE-Curve448 : 1 handshake/s ECDH-secp521r1 : 1 handshake/s ECDH-brainpoolP512r1 : 0 handshake/s ECDH-secp384r1 : 2 handshake/s ECDH-brainpoolP384r1 : 0 handshake/s ECDH-secp256r1 : 3 handshake/s ECDH-secp256k1 : 3 handshake/s ECDH-brainpoolP256r1 : 0 handshake/s ECDH-secp224r1 : 4 handshake/s ECDH-secp224k1 : 0 handshake/s ECDH-secp192r1 : 0 handshake/s ECDH-secp192k1 : 0 handshake/s ECDH-Curve25519 : 0 handshake/s ECDH-Curve448 : 2 handshake/s

[END]