erpc_matrix_multiply_mu
Overview
The Multicore eRPC Matrix Multiply project is a simple demonstration program that uses the MCUXpresso SDK software and the Multicore SDK to show how to implement the Remote Procedure Call between cores of the multicore system. The primary core (eRPC client) releases the secondary core (eRPC server) from the reset and then the erpcMatrixMultiply() eRPC call is issued to let the secondary core to perform the multiplication of two randomly generated matrices. The original matrices and the result matrix is printed out to the serial console by the primary core. The matrix multiplication can be issued repeatedly when pressing a SW board button. MU (Messaging Unit) erpc transport layer is used in this example application.
eRPC documentation
eRPC specific files are stored in: middleware\multicore\erpc eRPC documentation is stored in: middleware\multicore\erpc\doc eRPC is open-source project stored on github: https://github.com/EmbeddedRPC/erpc eRPC documentation can be also found in: http://embeddedrpc.github.io