This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

ele_symmetric

Overview

The ELE symmetric application provides example how to use SSSAPI to encrypt/decrypt data via AES.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

ELE Symmetric via SSSAPI Example

****************** Crypto AES-CBC ******************
AES-CBC crypto encryption success and output matches expected result.

AES-CBC crypto decryption success and output matches expected result.

****************** Crypto AES-GCM ******************
AES-GCM crypto encryption success and output matches expected result.

End of Example with SUCCESS!!

Example end

Supported Boards