This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

tfm_psatest_s

Overview

The Trusted Firmware M (TF-M) PSA Dev API test application provides verification that secure service API behaviours are implemented correctly. The PSA Dev API tests are the basis for getting the PSA Functional API Certification.

NOTE: The TF-M main() functions have a non-standard location: - Secure main() is in the tf-m\secure_fw\spm\cmsis_psa\main.c file. - Non-Secure main() is in the tf-m-tests\app\main_ns.c file.

Supported Boards