This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

secure_gpio_s

SECURE VULNERABILITY NOTE: There is a vulnerability that can affect TrustZone applications that also use floating point unit (CVE-2021-35465). The TrustZone examples delivered here do not use floating point, and so they aren’t affected. However, if TrustZone and FPU are used together, the used compiler should be checked for inbuilt workaround. If workaround is not available yet, then the actions described in CVE-2021-35465 should be applied manually.

Actual compilers status for this vulnerability: MCUX IDE v11.5.0 – fix not available yet GNU Arm Embedded Toolchain 10.3-2021.07 - fix not available yet EWARM v9.20.1 – already fixed ARM MDK v5.35 – check for new Arm compiler v6.17

Overview

The Secure GPIO demo application demonstrates using of secure GPIO peripheral and GPIO mask feature in AHB secure controller. The secure GPIO is standard GPIO peripheral supporting 32 pins on port 0 only. Having two GPIO peripherals allows user to configure one GPIO peripheral into secure world and another one into normal world. Thus for all pins on port 0, user can select whether the pin is controlled from secure or non-secure domain (using IOCON). Since the every GPIO pin allows to read its state regardless of its configuration, the AHB secure controller has build in feature GPIO mask for all GPIO pins. It is recommended to mask GPIO pins for all peripherals assigned to secure domain in order to eliminate information leak from GPIO pins. For example UART is assigned to secure world. But GPIO peripheral still allows to read state of TxD and RxD pins. This information can be use to decode UART communication from normal world, which can lead to unwanted information leak.

This Secure GPIO demo uses one user button (let’s call it LED button), which is read from both secure (using “secure” GPIO) and normal world (using “standard” GPIO), and two LED diodes, one controlled from secure and second one from normal world. Once LED button is pressed, both secure and non-secure worlds detect this user action (logical zero is read) and both LEDs are switched ON (first LED is controlled from secure world and second one from non-secure world). So both LEDs are controlled by LED button. The second part of the demo demonstrates AHB secure controller GPIO mask feature. This feature is controlled by second user button (let’s call it MASK button). If the MASK button is not pressed, the GPIO mask feature is disabled and normal world can read the state of LED button. Therefore LED button still controls both LEDs as described in previous paragraph. If the MASK button is pressed, the GPIO mask feature is enabled. In this case normal world cannot read state of state of first button and logical zero is read only. Since logical zero corresponds to pressed LED button, the LED, controlled from normal world, is immediately switched ON regardless of the state of LED button. The LED, controlled from secure world, can be still controlled by LED button, because the state of this button is still available to the secure world via GPIO assigned to secure world. Below is a table illustrating the individual button and LED states. For user buttons and LEDs assignment on particular board, see chapter “Running the demo”.

Input

OUTPUT

ALLOW button

LED button

“secure” LED

“normal” LED

PRESSED

RELEASED

ON

ON

RELEASED

RELEASED

OFF

OFF

PRESSED

PRESSED

ON

ON

RELEASED

PRESSED

OFF

ON

Supported Boards