This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Zephyr test plan

The following roughly describes how MCUboot is tested on Zephyr. The testing is done with the code in samples/zephyr. These examples were written using the FRDM-K64F, but other boards should be similar. At this time, however, the partitions are hardcoded in the Makefile targets to flash.

Note that the script “run-tests.sh” in that directory is helpful for automating the process, and provides simple “y or n” prompts for each test case and expected result.

Building and running.

The tests are build using the various test-* targets in samples/zephyr/Makefile. For each test, invoke make with that target:

$ make test-good-rsa

Begin by doing a full erase, and programming the bootloader itself:

$ pyocd erase --chip
$ make flash_boot

After it resets, look for “main: Starting bootloader”, a few debug messages, and lastly: “main: Unable to find bootable image”.

Then, load hello1:

$ make flash_hello1

This should print “main: Jumping to the first image slot”, and you should get an image “hello1”.

Note that there are comments with each test target describing the intended behavior for each of these steps. Sometimes an upgrade will happen and sometimes it will not.

$ make flash_hello2

This should print a message: boot_swap_type: Swap type: test, and you should see “hello2”.

Now reset the target::

$ pyocd commander -c reset

And you should see a revert and “hello1” running.

Testing that mark ok works

Repeat this, to make sure we can mark the image as OK, and that a revert doesn’t happen:

$ make flash_hello1
$ make flash_hello2

We should have just booted the hello2. Mark this as OK:

$ pyocd flash -a 0x7ffe8 image_ok.bin
$ pyocd commander -c reset

And make sure this stays in the “hello2” image.

This step doesn’t make sense on the tests where the upgrade doesn’t happen.

Testing all configurations

Repeat these steps for each of the test-* targest in the Makefile.