This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

coreMQTT Agent Library

The coreMQTT Agent library is a high level API that adds thread safety to the coreMQTT library. The library provides thread safe equivalents to the coreMQTT’s APIs, greatly simplifying its use in multi-threaded environments. The coreMQTT Agent library manages the MQTT connection by serializing the access to the coreMQTT library and reducing implementation overhead (e.g., removing the need for the application to repeatedly call to MQTT_ProcessLoop). This allows your multi-threaded applications to share the same MQTT connection, and enables you to design an embedded application without having to worry about coreMQTT thread safety.

This library has gone through code quality checks including verification that no function has a GNU Complexity score over 8, and checks against deviations from mandatory rules in the MISRA coding standard. Deviations from the MISRA C:2012 guidelines are documented under MISRA Deviations. This library has also undergone both static code analysis from Coverity static analysis, and validation of memory safety through the CBMC automated reasoning tool.

See memory requirements for this library here.

Cloning this repository

This repo uses Git Submodules to bring in dependent components.

To clone using HTTPS:

git clone https://github.com/FreeRTOS/coreMQTT-Agent.git --recurse-submodules

Using SSH:

git clone git@github.com:FreeRTOS/coreMQTT-Agent.git --recurse-submodules

If you have downloaded the repo without using the --recurse-submodules argument, you need to run:

git submodule update --init --recursive

coreMQTT Agent Library Configurations

The MQTT Agent library uses the same core_mqtt_config.h configuration file as coreMQTT, with the addition of configuration constants listed at the top of core_mqtt_agent.h and core_mqtt_agent_command_functions.h. Documentation for these configurations can be found here.

To provide values for these configuration values, they must be either:

  • Defined in core_mqtt_config.h used by coreMQTT OR

  • Passed as compile time preprocessor macros

Porting the coreMQTT Agent Library

In order to use the MQTT Agent library on a platform, you need to supply thread safe functions for the agent’s messaging interface.

Messaging Interface

Each of the following functions must be thread safe.

Function Pointer

Description

MQTTAgentMessageSend_t

A function that sends commands (as MQTTAgentCommand_t * pointers) to be received by MQTTAgent_CommandLoop. This can be implemented by pushing to a thread safe queue.

MQTTAgentMessageRecv_t

A function used by MQTTAgent_CommandLoop to receive MQTTAgentCommand_t * pointers that were sent by API functions. This can be implemented by receiving from a thread safe queue.

MQTTAgentCommandGet_t

A function that returns a pointer to an allocated MQTTAgentCommand_t structure, which is used to hold information and arguments for a command to be executed in MQTTAgent_CommandLoop(). If using dynamic memory, this can be implemented using malloc().

MQTTAgentCommandRelease_t

A function called to indicate that a command structure that had been allocated with the MQTTAgentCommandGet_t function pointer will no longer be used by the agent, so it may be freed or marked as not in use. If using dynamic memory, this can be implemented with free().

Reference implementations for the interface functions can be found in the reference examples below.

Additional Considerations

Static Memory

If only static allocation is used, then the MQTTAgentCommandGet_t and MQTTAgentCommandRelease_t could instead be implemented with a pool of MQTTAgentCommand_t structures, with a queue or semaphore used to control access and provide thread safety. The below reference examples use static memory with a command pool.

Subscription Management

The MQTT Agent does not track subscriptions for MQTT topics. The receipt of any incoming PUBLISH packet will result in the invocation of a single MQTTAgentIncomingPublishCallback_t callback, which is passed to MQTTAgent_Init() for initialization. If it is desired for different handlers to be invoked for different incoming topics, then the publish callback will have to manage subscriptions and fan out messages. A platform independent subscription manager example is implemented in the reference examples below.

Building the Library

You can build the MQTT Agent source files that are in the source directory, and add source/include to your compiler’s include path. Additionally, the MQTT Agent library requires the coreMQTT library, whose files follow the same source/ and source/include pattern as the agent library; its build instructions can be found here.

If using CMake, the mqttAgentFilePaths.cmake file contains the above information of the source files and the header include path from this repository. The same information is found for coreMQTT from mqttFilePaths.cmake in the coreMQTT submodule.

For a CMake example of building the MQTT Agent library with the mqttAgentFilePaths.cmake file, refer to the coverity_analysis library target in test/CMakeLists.txt file.

Building Unit Tests

Checkout CMock Submodule

To build unit tests, the submodule dependency of CMock is required. Use the following command to clone the submodule:

git submodule update --checkout --init --recursive test/unit-test/CMock

Unit Test Platform Prerequisites

  • For running unit tests

    • C90 compiler like gcc

    • CMake 3.13.0 or later

    • Ruby 2.0.0 or later is additionally required for the CMock test framework (that we use).

  • For running the coverage target, gcov and lcov are additionally required.

Steps to build Unit Tests

  1. Go to the root directory of this repository. (Make sure that the CMock submodule is cloned as described above)

  2. Run the cmake command: cmake -S test -B build

  3. Run this command to build the library and unit tests: make -C build all

  4. The generated test executables will be present in build/bin/tests folder.

  5. Run cd build && ctest to execute all tests and view the test run summary.

CBMC

To learn more about CBMC and proofs specifically, review the training material here.

The test/cbmc/proofs directory contains CBMC proofs.

In order to run these proofs you will need to install CBMC and other tools by following the instructions here.

Reference examples

Please refer to the demos of the MQTT Agent library in the following locations for reference examples on FreeRTOS platforms:

Location

coreMQTT Agent Demos

FreeRTOS/FreeRTOS

Documentation

The MQTT Agent API documentation can be found here.

Generating documentation

The Doxygen references were created using Doxygen version 1.9.2. To generate the Doxygen pages yourself, please run the following command from the root of this repository:

doxygen docs/doxygen/config.doxyfile

Getting help

You can use your Github login to get support from both the FreeRTOS community and directly from the primary FreeRTOS developers on our active support forum. You can find a list of frequently asked questions here.

Contributing

See CONTRIBUTING.md for information on contributing.

License

This library is licensed under the MIT License. See the LICENSE file.