Build an example application
Perform the following steps to build the hello_world
example application.
Open the desired demo application workspace. Most example application workspace files can be located using the following path:
<install_dir>/boards/<board_name>/<example_type>/<application_name>/iar
Using the FRDM-K32L2A4S hardware platform as an example, the
hello_world
workspace is located in:<install_dir>/boards/frdmk32l2a4s/demo_apps/hello_world/iar/hello_world.eww
Select the desired build target from the drop-down menu. For this example, select the hello_world – debug target.
To build the demo application, click the Make button highlighted in red below.
The build completes without errors.
Parent topic:Run a demo application using IAR