Build an example application
To build an example application, follow these steps.
Drag and drop the SDK zip file into the Installed SDKs view to install an SDK. In the window that appears, click OK and wait until the import has finished.
On the Quickstart Panel, click Import SDK example(s)….
In the window that appears, expand the K32L2 folder and select K32L2A41xxxxA. Then, select frdmk32l2a4s and click Next.
Expand the demo_apps folder and select hello_world. Then, click Next.
Ensure the option of
Redlib: Use floating point version of printf
is selected if the cases’ print floating point numbers are on the terminal for demo applications such as . Otherwise, it is not necessary to select this option. Then, click Finish.
Parent topic:Run a demo using MCUXpresso IDE