Build an XIP example application

  1. Following the same steps as Section 5.3, “Run an non-xip (plain load) example application”, type “build_debug.bat” on the command line or double click the “build_debug.bat” file in Windows Explorer to perform the build.

  2. The build output is shown in this figure:

Parent topic:Run a demo using Arm® GCC