Build an example application {#GUID-151EFC23-F84E-4EB4-8940-5A8E58C7E348}
Do the following steps to build the hello_world
example application.
Open the desired demo application workspace. Most example application workspace files can be located using the following path:
<install_dir>/boards/<board_name>/<example_type>/<application_name>/iar
Using the LPCXpresso55S69 hardware platform as an example, the
hello_world
workspace is located in:<install_dir>/boards/lpcxpresso55s69/demo_apps/hello_world/iar/hello_world.eww
Other example applications may have additional folders in their path.
Select the desired build target from the drop-down menu.
For this example, select hello_world – debug.
|
|
To build the demo application, click Make, highlighted in red in Figure 2.
|
|
The build completes without errors.
Parent topic:Run a demo application using IAR