Run an example application {#GUID-B4CDD55E-3A4B-4121-BE6F-BE8492E9669F}

To download and run the application, perform these steps:

  1. See the table in Default debug interfaces to determine the debug interface that comes loaded on your specific hardware platform.

  2. Connect the development platform to your PC via USB cable using OpenSDA USB connector.

  3. Open the terminal application on the PC, such as PuTTY or TeraTerm and connect to the debug serial port number (to determine the COM port number, see How to determine COM port). Configure the terminal with these settings:

    1. 115200 or 9600 baud rate, depending on your board (reference BOARD_DEBUG_UART_BAUDRATE variable in the board.h file)

    2. No parity

    3. 8 data bits

    4. 1 stop bit |

|

  1. In μVision, after the application is built, click the Download button to download the application to the target.

  2. After clicking the Download button, the application downloads to the target and is running. To debug the application, click the Start/Stop Debug Session button, highlighted in red.

    |

|

  1. Run the code by clicking the Run button to start the application.

    |

|

The `hello_world` application is now running and a banner is displayed on the terminal. If this does not appear, check your terminal settings and connections.

|![](../images/text_display_hello_world.png "Text display of the hello_world demo")

|

Note: Must use J-Link v6.56a or higher version in Keil. When using J-Link on Keil, if the device is blank (flash is erased), first uncomment the line16 in the example/mdk/JLinkSettings.JLinkScript to release the function void ResetTarget(void){}. Then do the download or debug, comment the function void ResetTarget(void){} again.

Parent topic:Run a demo using Keil MDK/μVision