Build an example application
Do the following steps to build the hello_world
example application.
Open the desired demo application workspace. Most example application workspace files can be located using the following path:
<install_dir>/boards/<board_name>/<example_type>/<application_name>/iar
Using the IMXRT1050-EVKB hardware platform as an example, the
hello_world
workspace is located in:><install_dir>/boards/evkbimxrt1050/demo_apps/hello_world/iar/hello_world.eww
Other example applications may have additional folders in their path.
Select the desired build target from the drop-down menu.
There are twelve project configurations (build targets) supported for most MCUXpresso SDK projects:
Debug
– Compiler optimization is set to low, and debug information is generated for the executable. The linker file isRAM
linker, where text and data section is put in internal TCM.Release
– Compiler optimization is set to high, and debug information is not generated. The linker file isRAM
linker, where text and data section is put in internal TCM.ram_0x1400_debug
– Project configuration is same as the debug target. The linker file isRAM_0x1400
linker, where text is put in ITCM with offset 0x1400 and data put in DTCM.ram_0x1400_release
– Project configuration is same as the release target. The linker file isRAM_0x1400
linker, where text is put in ITCM with offset 0x1400 and data put in DTCM.sdram_debug
– Project configuration is same as the debug target. The linker file isSDRAM
linker, where text is put in internal TCM and data put in SDRAM.sdram_release
– Project configuration is same as the release target. The linker file isSDRAM
linker, where text is put in internal TCM and data put in SDRAM.sdram_txt_debug
– Project configuration is same as the debug target. The linker file isSDRAM_txt
linker, where text is put in SDRAM and data put in OCRAM.sdram_txt_release
– Project configuration is same as the release target. The linker file isSDRAM_txt
linker, where text is put in SDRAM and data put in OCRAM.flexspi_nor_debug
– Project configuration is same as the debug target. The linker file isflexspi_nor
linker, where text is put in flash and data put in TCM.flexspi_nor_release
– Project configuration is same as the release target. The linker file isflexspi_nor
linker, where text is put in flash and data put in TCM.flexspi_nor_sdram_release
- Project configuration is same as the release target. The linker file isflexspi_nor_sdram
linker, where text is put in flash and data put in SDRAM.flexspi_nor_sdram_debug
– Project configuration is same as the debug target. The linker file isflexspi_nor_sdram
linker, where text is put in flash and data put in SDRAM. For some examples need large data memory, onlysdram_debug
andsdram_release
targets are supported.
For this example, select hello_world – debug.
To build the demo application, click Make, highlighted in red in Figure 2.
The build completes without errors.
Parent topic:Run a demo application using IAR