Build an example application
To build an example application, follow these steps.
Drag and drop the SDK zip file into the Installed SDKs view to install the MCUXpresso SDK. In the window that appears, click OK and wait until the import has finished.
|
|
On the Quickstart Panel, click Import SDK example(s)…, as shown in Figure 2.
|
|
In the window that appears, expand the MIMXRT1024folder and select MIMXRT1024xxxxx. Then, select evkmimxrt1024 and click Next, as shown in Figure 3.
|
|
Expand the
demo_apps
folder, selecthello_world
, and then click Next.Ensure the option Redlib: Use floating-point version of printf is selected if the cases print floating-point numbers on the terminal (for demo applications such as
dac32_adc12
,dac_adc
,dac_cadc
,ecompass
,sai
,coremark
,mbedtls_benchmark
,wolfssl_benchmark
, and formmcau_examples
such asmmcau_api
). Otherwise, there is no need to select it. Click Finish.|
|
**Note:** If you want to use semihost to print log, first select the **Semihost** button when importing projects, as shown in [Figure 5](build_an_example_application.md#FLOAATING).
|
|
On the Quickstart panel, click build
evkmimxrt1024\_demo\_apps\_hello\_world \[Debug\]
, as shown in Figure 6.|
|
Parent topic:Run a demo using MCUXpresso IDE