Install License Key
Xtensa development tools use FLEXlm for license management. FLEXlm licensing is required for tools such as the Xtensa Xplorer IDE, Xtensa C and C++ compiler, and Instruction Set Simulator (ISS).
Currently RT600 supports node-locked license for Xtensa tools. A node-locked license permits tools to run on a specific computer, tied to the MAC address of the primary network interface permanently attached to the machine.
Identify PC MAC Address
To generate the correct license file, you should first identify the appropriate MAC for the computer you plan to run Xtensa tools on. Remove ‘-‘ or ‘:’ symbols in the MAC address.
Windows:
|
|
Linux:
|
|
Note: For Linux: MAC address must be associated with eth0 interface. If not, FLEXlm cannot perform the license checkout, compilation, or simulation of code is not possible. If the host has the MAC address associated with another interface, for example em1, the following approach may be used.
# Add udev rule for naming interface
$ sudo vim /etc/udev/rules.d/70-persistent-net.rules
# udev rule (replace ‘XX’ with the MAC address of your PC):
SUBSYSTEM=="net", ACTION=="add", ATTR{address}=="XX:XX:XX:XX:XX:XX", NAME="eth0"
# Change "em1" to "eth0" in your interfaces file.
$ sudo vim /etc/network/interfaces
# Restart udev or reboot machine
$ sudo reboot
Alternatively, you can use the approach recommended by your IT team to rename the interface to eth0.
Parent topic:Install License Key
Download License Key
To download the license key:
Reload or return to the Tensilica URL: https://tensilicatools.com/download/rt600-download-page/.
Click the button and get the license key for RT600 SDK.
|
|
Provide the address.
|
|
Once the license file has been generated and downloaded, open your recently installed Xplorer V10.1.11.
Select menu Help > Xplorer License Keys > Install Software Keys.
Select the license key file.
|
|
Click the Finish button.
Note: The generated license file only supports debug/run on the RT600 device target. It does not support software simulation/Xplorer ISS. If you have special requirements to run the software simulations, contact Cadence directly.
Parent topic:Install License Key
Parent topic:Install Xplorer Toolchains