Logo
25.03.00-pvw2
MCUXpresso SDK Project v: latest
Document Release Versions
24.12.00-pvw2
24.12.00
25.03.00-pvw2

Introduction

  • MCUXpresso SDK
  • Setup

Getting Started

  • Github Repository
  • Zip Package

User Guide

  • Drivers
  • Examples
  • Middlewares
  • RTOS
  • Boards
    • DSC
    • Kinetis
    • LPC
    • MCX
    • i.MX RT
    • Wireless
      • FRDM-RW612
        • Overview
        • Getting Started
          • Getting Started with MCUXpresso SDK for FRDM-RW612
        • Release Notes
      • K32W148-EVK
      • KW45B41Z-EVK
      • KW45B41Z-LOC
      • KW47-EVK
      • KW47-LOC
      • RD-RW612-BGA
    • i.MX

Development

  • Architecture
  • Developing with MCUXpresso SDK
  • Build And Configuration System
  • Documentation

Releases

  • Release Notes
mcuxsdk
  • Docs / 25.03.00-pvw2 »
  • Supported Boards »
  • Wireless »
  • FRDM-RW612 »
  • Getting Started with MCUXpresso SDK for FRDM-RW612
  • Open on Repo Report an issue with this page

Getting Started with MCUXpresso SDK for FRDM-RW612

Table of Contents

  • Overview
  • MCUXpresso SDK board support package folders
    • Example application structure
    • Locating example application source files
  • Run a demo using MCUXpresso IDE
    • Select the workspace location
    • Build an example application
    • Run an example application
  • Run a demo application using IAR
    • Build an example application
    • Run an example application
    • IAR RAM debugging notes
  • Run a demo using Arm GCC
    • Set up toolchain
      • Install GCC Arm Embedded tool chain
      • Install MinGW (only required on Windows OS)
      • Add a new system environment variable for ARMGCC_DIR
      • Install CMake
    • Build an example application
    • Run an example application
  • Run a demo using Keil MDK/μVision
    • Install CMSIS device pack
    • Build an example application
    • Run an example application
  • MCUXpresso IDE New Project Wizard
  • How to determine COM port
  • How to define IRQ handler in CPP files
  • Default debug interfaces
  • Updating debugger firmware
    • Updating OpenSDA firmware
    • Updating MCU-Link firmware

Copyright 2025, NXP. Last generated on Mar 06, 2025 09:10+0100; branch release/25.03.00-pvw2, revision 8403f88d835055ff0db6da35e9b065b324249514.